Other Parts Discussed in Thread: TPS65910
I was using the AM3352BZCZD80 and the TPS65217CRSLR to produce the product.
However, the PMIC of the part cannot be obtained, so the production is quite difficult.
So, I would like to inquire about the above.
1) Are there any parts that can support pin to pin?
2) If the package is different, I have idea to solve it by changing the PCB. The TPS65910 on the website seems to be in TI's inventory, can I use it?
- If it is possible to use the TPS65910, is it possible to use it without changing the PMIC software?
Your help is desperately needed.
thank you.