Part Number: AM3354
Hi,
linux 3.2
The customized board ADC AN7 read data abnormally, AIN0-6 are normal, AIN7 will occasionally appear a large negative value and each time it is a fixed value -550525552.

The voltage range is normal 0-1.8V, and the measured waveform has no abnormal changes.
Below is his driver ti_adc.c
/*
* TI ADC MFD driver
*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or
* modify it under the terms of the GNU General Public License as
* published by the Free Software Foundation version 2.
*
* This program is distributed "as is" WITHOUT ANY WARRANTY of any
* kind, whether express or implied; without even the implied warranty
* of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*/
#include <linux/init.h>
#include <linux/kernel.h>
#include <linux/err.h>
#include <linux/module.h>
#include <linux/slab.h>
#include <linux/interrupt.h>
#include <linux/platform_device.h>
#include <linux/io.h>
#include <linux/sched.h>
#include "../iio.h"
#include "../sysfs.h"
#include "../buffer_generic.h"
#include "../ring_sw.h"
#include <linux/mfd/ti_tscadc.h>
#include <linux/platform_data/ti_adc.h>
struct adc_device {
struct ti_tscadc_dev *mfd_tscadc;
struct iio_dev *idev;
struct work_struct poll_work;
wait_queue_head_t wq_data_avail;
int channels;
int irq;
bool is_continuous_mode;
u16 *buffer;
};
static unsigned int adc_readl(struct adc_device *adc, unsigned int reg)
{
return readl(adc->mfd_tscadc->tscadc_base + reg);
}
static void adc_writel(struct adc_device *adc, unsigned int reg,
unsigned int val)
{
writel(val, adc->mfd_tscadc->tscadc_base + reg);
}
static void adc_step_config(struct adc_device *adc_dev, bool mode)
{
unsigned int stepconfig;
int i, channels = 0, steps;
/*
* There are 16 configurable steps and 8 analog input
* lines available which are shared between Touchscreen and ADC.
*
* Steps backwards i.e. from 16 towards 0 are used by ADC
* depending on number of input lines needed.
* Channel would represent which analog input
* needs to be given to ADC to digitalize data.
*/
steps = TOTAL_STEPS - adc_dev->channels;
channels = TOTAL_CHANNELS - adc_dev->channels;
if (mode == 0)
stepconfig = TSCADC_STEPCONFIG_AVG_16 | TSCADC_STEPCONFIG_FIFO1;
else
stepconfig = TSCADC_STEPCONFIG_AVG_16 | TSCADC_STEPCONFIG_FIFO1
| TSCADC_STEPCONFIG_MODE_SWCNT;
for (i = (steps + 1); i <= TOTAL_STEPS; i++) {
adc_writel(adc_dev, TSCADC_REG_STEPCONFIG(i),
stepconfig | TSCADC_STEPCONFIG_INP(channels));
adc_writel(adc_dev, TSCADC_REG_STEPDELAY(i),
TSCADC_STEPCONFIG_OPENDLY);
channels++;
}
}
static ssize_t tiadc_show_mode(struct device *dev,
struct device_attribute *attr, char *buf)
{
struct iio_dev *indio_dev = dev_get_drvdata(dev);
struct adc_device *adc_dev = iio_priv(indio_dev);
unsigned int tmp;
tmp = adc_readl(adc_dev, TSCADC_REG_STEPCONFIG(TOTAL_STEPS));
tmp &= TSCADC_STEPCONFIG_MODE(1);
if (tmp == 0x00)
return sprintf(buf, "oneshot\n");
else if (tmp == 0x01)
return sprintf(buf, "continuous\n");
else
return sprintf(buf, "Operation mode unknown\n");
}
static ssize_t tiadc_set_mode(struct device *dev,
struct device_attribute *attr, const char *buf, size_t count)
{
struct iio_dev *indio_dev = dev_get_drvdata(dev);
struct adc_device *adc_dev = iio_priv(indio_dev);
unsigned int config;
config = adc_readl(adc_dev, TSCADC_REG_CTRL);
config &= ~(TSCADC_CNTRLREG_TSCSSENB);
adc_writel(adc_dev, TSCADC_REG_CTRL, config);
if (!strncmp(buf, "oneshot", 7))
adc_dev->is_continuous_mode = false;
else if (!strncmp(buf, "continuous", 10))
adc_dev->is_continuous_mode = true;
else {
dev_err(dev, "Operational mode unknown\n");
return -EINVAL;
}
adc_step_config(adc_dev, adc_dev->is_continuous_mode);
config = adc_readl(adc_dev, TSCADC_REG_CTRL);
adc_writel(adc_dev, TSCADC_REG_CTRL,
(config | TSCADC_CNTRLREG_TSCSSENB));
return count;
}
static IIO_DEVICE_ATTR(mode, S_IRUGO | S_IWUSR, tiadc_show_mode,
tiadc_set_mode, 0);
static struct attribute *tiadc_attributes[] = {
&iio_dev_attr_mode.dev_attr.attr,
NULL,
};
static const struct attribute_group tiadc_attribute_group = {
.attrs = tiadc_attributes,
};
static irqreturn_t tiadc_irq(int irq, void *private)
{
struct iio_dev *idev = private;
struct adc_device *adc_dev = iio_priv(idev);
unsigned int status, config;
status = adc_readl(adc_dev, TSCADC_REG_IRQSTATUS);
if (status & TSCADC_IRQENB_FIFO1OVRRUN) {
config = adc_readl(adc_dev, TSCADC_REG_CTRL);
config &= ~(TSCADC_CNTRLREG_TSCSSENB);
adc_writel(adc_dev, TSCADC_REG_CTRL, config);
adc_writel(adc_dev, TSCADC_REG_IRQSTATUS,
TSCADC_IRQENB_FIFO1OVRRUN |
TSCADC_IRQENB_FIFO1UNDRFLW |
TSCADC_IRQENB_FIFO1THRES);
adc_writel(adc_dev, TSCADC_REG_CTRL,
(config | TSCADC_CNTRLREG_TSCSSENB));
return IRQ_HANDLED;
} else if (status & TSCADC_IRQENB_FIFO1THRES) {
adc_writel(adc_dev, TSCADC_REG_IRQCLR,
TSCADC_IRQENB_FIFO1THRES);
if (iio_buffer_enabled(idev)) {
if (!work_pending(&adc_dev->poll_work))
schedule_work(&adc_dev->poll_work);
} else {
wake_up_interruptible(&adc_dev->wq_data_avail);
}
return IRQ_HANDLED;
} else {
return IRQ_NONE;
}
}
static void tiadc_poll_handler(struct work_struct *work_s)
{
struct adc_device *adc_dev =
container_of(work_s, struct adc_device, poll_work);
struct iio_dev *idev = iio_priv_to_dev(adc_dev);
struct iio_buffer *buffer = idev->buffer;
unsigned int fifo1count, readx1;
int i;
u32 *iBuf;
fifo1count = adc_readl(adc_dev, TSCADC_REG_FIFO1CNT);
if (fifo1count * sizeof(u32) <
buffer->access->get_bytes_per_datum(buffer)) {
dev_err(adc_dev->mfd_tscadc->dev, "%s: Short FIFO event\n",
__func__);
goto out;
}
iBuf = kmalloc(fifo1count * sizeof(u32), GFP_KERNEL);
if (iBuf == NULL)
goto out;
for (i = 0; i < fifo1count; i++) {
readx1 = adc_readl(adc_dev, TSCADC_REG_FIFO1);
readx1 &= TSCADC_FIFOREAD_DATA_MASK;
iBuf[i] = readx1;
}
buffer->access->store_to(buffer, (u8 *) iBuf, iio_get_time_ns());
kfree(iBuf);
out:
adc_writel(adc_dev, TSCADC_REG_IRQSTATUS,
TSCADC_IRQENB_FIFO1THRES);
adc_writel(adc_dev, TSCADC_REG_IRQENABLE,
TSCADC_IRQENB_FIFO1THRES);
}
static int tiadc_buffer_preenable(struct iio_dev *idev)
{
struct iio_buffer *buffer = idev->buffer;
buffer->access->set_bytes_per_datum(buffer, 16);
return 0;
}
static int tiadc_buffer_postenable(struct iio_dev *idev)
{
struct adc_device *adc_dev = iio_priv(idev);
struct iio_buffer *buffer = idev->buffer;
unsigned int enb, config;
int stepnum;
u8 bit;
if (!adc_dev->is_continuous_mode) {
pr_info("Data cannot be read continuously in one shot mode\n");
return -EINVAL;
} else {
config = adc_readl(adc_dev, TSCADC_REG_CTRL);
adc_writel(adc_dev, TSCADC_REG_CTRL,
config & ~TSCADC_CNTRLREG_TSCSSENB);
adc_writel(adc_dev, TSCADC_REG_CTRL,
config | TSCADC_CNTRLREG_TSCSSENB);
adc_writel(adc_dev, TSCADC_REG_IRQSTATUS,
TSCADC_IRQENB_FIFO1THRES |
TSCADC_IRQENB_FIFO1OVRRUN |
TSCADC_IRQENB_FIFO1UNDRFLW);
adc_writel(adc_dev, TSCADC_REG_IRQENABLE,
TSCADC_IRQENB_FIFO1THRES |
TSCADC_IRQENB_FIFO1OVRRUN);
adc_writel(adc_dev, TSCADC_REG_SE, 0x00);
for_each_set_bit(bit, buffer->scan_mask,
adc_dev->channels) {
struct iio_chan_spec const *chan = idev->channels + bit;
/*
* There are a total of 16 steps available
* that are shared between ADC and touchscreen.
* We start configuring from step 16 to 0 incase of
* ADC. Hence the relation between input channel
* and step for ADC would be as below.
*/
stepnum = chan->channel + 9;
enb = adc_readl(adc_dev, TSCADC_REG_SE);
enb |= (1 << stepnum);
adc_writel(adc_dev, TSCADC_REG_SE, enb);
}
return 0;
}
}
static int tiadc_buffer_postdisable(struct iio_dev *idev)
{
struct adc_device *adc_dev = iio_priv(idev);
adc_writel(adc_dev, TSCADC_REG_IRQCLR, (TSCADC_IRQENB_FIFO1THRES |
TSCADC_IRQENB_FIFO1OVRRUN |
TSCADC_IRQENB_FIFO1UNDRFLW));
adc_writel(adc_dev, TSCADC_REG_SE, TSCADC_STPENB_STEPENB_TC);
return 0;
}
static const struct iio_buffer_setup_ops tiadc_swring_setup_ops = {
.preenable = &tiadc_buffer_preenable,
.postenable = &tiadc_buffer_postenable,
.postdisable = &tiadc_buffer_postdisable,
};
static int tiadc_config_sw_ring(struct iio_dev *idev)
{
struct adc_device *adc_dev = iio_priv(idev);
int ret;
idev->buffer = iio_sw_rb_allocate(idev);
if (!idev->buffer)
ret = -ENOMEM;
idev->buffer->access = &ring_sw_access_funcs;
idev->buffer->setup_ops = &tiadc_swring_setup_ops;
INIT_WORK(&adc_dev->poll_work, &tiadc_poll_handler);
idev->modes |= INDIO_BUFFER_HARDWARE;
return 0;
}
static int tiadc_channel_init(struct iio_dev *idev, struct adc_device *adc_dev)
{
struct iio_chan_spec *chan_array;
int i, channels;
idev->num_channels = adc_dev->channels;
chan_array = kcalloc(idev->num_channels, sizeof(struct iio_chan_spec),
GFP_KERNEL);
if (chan_array == NULL)
return -ENOMEM;
channels = TOTAL_CHANNELS - adc_dev->channels;
for (i = 0; i < (idev->num_channels); i++) {
struct iio_chan_spec *chan = chan_array + i;
chan->type = IIO_VOLTAGE;
chan->indexed = 1;
chan->channel = channels;
chan->scan_index = i;
chan->scan_type.sign = 'u';
chan->scan_type.realbits = 12;
chan->scan_type.storagebits = 32;
chan->scan_type.shift = 0;
channels++;
}
idev->channels = chan_array;
return idev->num_channels;
}
static void tiadc_channel_remove(struct iio_dev *idev)
{
kfree(idev->channels);
}
static int tiadc_read_raw(struct iio_dev *idev,
struct iio_chan_spec const *chan,
int *val, int *val2, long mask)
{
struct adc_device *adc_dev = iio_priv(idev);
int i, map_val, tmp;
unsigned int fifo1count, readx1, stepid;
unsigned long timeout = jiffies + usecs_to_jiffies
(IDLE_TIMEOUT * adc_dev->channels);
if (adc_dev->is_continuous_mode) {
pr_info("One shot mode not enabled\n");
return -EINVAL;
} else {
if(adc_dev->channels == 4)
tmp = (1 << (chan->channel + TOTAL_CHANNELS + 1)) | TSCADC_STPENB_STEPENB_TC;
else
tmp = (1 << (chan->channel + TOTAL_CHANNELS + 1));
adc_writel(adc_dev, TSCADC_REG_SE, tmp);
/* Wait for ADC sequencer to complete sampling */
while (adc_readl(adc_dev, TSCADC_REG_ADCFSM) &
TSCADC_SEQ_STATUS) {
if (time_after(jiffies, timeout))
return -EAGAIN;
}
map_val = chan->channel + TOTAL_CHANNELS;
*val = -1;
timeout = jiffies + usecs_to_jiffies
(IDLE_TIMEOUT * adc_dev->channels);
while(1){
fifo1count = adc_readl(adc_dev, TSCADC_REG_FIFO1CNT);
if(!fifo1count){
if (time_after(jiffies, timeout)){
printk("wait fifo timeout\n");
return -EAGAIN;
} else
continue;
}
for (i = 0; i < fifo1count; i++) {
readx1 = adc_readl(adc_dev, TSCADC_REG_FIFO1);
stepid = readx1 & TSCADC_FIFOREAD_CHNLID_MASK;
stepid = stepid >> 0x10;
if (stepid == map_val) {
readx1 = readx1 & TSCADC_FIFOREAD_DATA_MASK;
*val = readx1;
}
}
if(*val != -1){
break;
}
}
return IIO_VAL_INT;
}
}
static const struct iio_info tiadc_info = {
.read_raw = &tiadc_read_raw,
.attrs = &tiadc_attribute_group,
};
static int __devinit tiadc_probe(struct platform_device *pdev)
{
struct iio_dev *idev;
struct adc_device *adc_dev = NULL;
struct ti_tscadc_dev *tscadc_dev = pdev->dev.platform_data;
struct mfd_tscadc_board *pdata;
int err;
pdata = (struct mfd_tscadc_board *)tscadc_dev->dev->platform_data;
if (!pdata || !pdata->adc_init) {
dev_err(tscadc_dev->dev, "Could not find platform data\n");
return -EINVAL;
}
idev = iio_allocate_device(sizeof(struct adc_device));
if (idev == NULL) {
dev_err(&pdev->dev, "failed to allocate iio device.\n");
err = -ENOMEM;
goto err_ret;
}
adc_dev = iio_priv(idev);
tscadc_dev->adc = adc_dev;
adc_dev->mfd_tscadc = tscadc_dev;
adc_dev->idev = idev;
adc_dev->channels = pdata->adc_init->adc_channels;
adc_dev->irq = tscadc_dev->irq;
idev->dev.parent = &pdev->dev;
idev->name = dev_name(&pdev->dev);
idev->modes = INDIO_DIRECT_MODE;
idev->info = &tiadc_info;
/* by default driver comes up with oneshot mode */
adc_step_config(adc_dev, adc_dev->is_continuous_mode);
/* program FIFO threshold to value minus 1 */
adc_writel(adc_dev, TSCADC_REG_FIFO1THR, FIFO1_THRESHOLD);
err = tiadc_channel_init(idev, adc_dev);
if (err < 0)
goto err_free_device;
init_waitqueue_head(&adc_dev->wq_data_avail);
err = request_irq(adc_dev->irq, tiadc_irq, IRQF_SHARED,
idev->name, idev);
if (err)
goto err_cleanup_channels;
err = tiadc_config_sw_ring(idev);
if (err)
goto err_free_irq;
err = iio_buffer_register(idev,
idev->channels, idev->num_channels);
if (err < 0)
goto err_free_sw_rb;
err = iio_device_register(idev);
if (err)
goto err_unregister;
dev_info(&pdev->dev, "attached adc driver\n");
platform_set_drvdata(pdev, idev);
return 0;
err_unregister:
iio_buffer_unregister(idev);
err_free_sw_rb:
iio_sw_rb_free(idev->buffer);
err_free_irq:
free_irq(adc_dev->irq, idev);
err_cleanup_channels:
tiadc_channel_remove(idev);
err_free_device:
iio_free_device(idev);
err_ret:
return err;
}
static int __devexit tiadc_remove(struct platform_device *pdev)
{
struct ti_tscadc_dev *tscadc_dev = pdev->dev.platform_data;
struct adc_device *adc_dev = tscadc_dev->adc;
struct iio_dev *idev = adc_dev->idev;
free_irq(adc_dev->irq, idev);
iio_device_unregister(idev);
iio_buffer_unregister(idev);
iio_sw_rb_free(idev->buffer);
tiadc_channel_remove(idev);
tscadc_dev->adc = NULL;
iio_free_device(idev);
platform_set_drvdata(pdev, NULL);
return 0;
}
static int adc_suspend(struct platform_device *pdev, pm_message_t state)
{
struct ti_tscadc_dev *tscadc_dev = pdev->dev.platform_data;
struct adc_device *adc_dev = tscadc_dev->adc;
unsigned int idle;
if (!device_may_wakeup(tscadc_dev->dev)) {
idle = adc_readl(adc_dev, TSCADC_REG_CTRL);
idle &= ~(TSCADC_CNTRLREG_TSCSSENB);
adc_writel(adc_dev, TSCADC_REG_CTRL, (idle |
TSCADC_CNTRLREG_POWERDOWN));
}
return 0;
}
static int adc_resume(struct platform_device *pdev)
{
struct ti_tscadc_dev *tscadc_dev = pdev->dev.platform_data;
struct adc_device *adc_dev = tscadc_dev->adc;
unsigned int restore;
restore = adc_readl(adc_dev, TSCADC_REG_CTRL);
restore &= ~(TSCADC_CNTRLREG_TSCSSENB);
adc_writel(adc_dev, TSCADC_REG_CTRL, restore);
adc_writel(adc_dev, TSCADC_REG_FIFO1THR, FIFO1_THRESHOLD);
adc_step_config(adc_dev, adc_dev->is_continuous_mode);
/* Make sure ADC is powered up */
restore &= ~(TSCADC_CNTRLREG_POWERDOWN);
restore |= TSCADC_CNTRLREG_TSCSSENB;
adc_writel(adc_dev, TSCADC_REG_CTRL, restore);
return 0;
}
static struct platform_driver tiadc_driver = {
.driver = {
.name = "tiadc",
.owner = THIS_MODULE,
},
.probe = tiadc_probe,
.remove = __devexit_p(tiadc_remove),
.suspend = adc_suspend,
.resume = adc_resume,
};
module_platform_driver(tiadc_driver);
MODULE_DESCRIPTION("TI ADC controller driver");
MODULE_AUTHOR("Rachna Patil <rachna@ti.com>");
MODULE_LICENSE("GPL");



Please give some suggestions.