Other Parts Discussed in Thread: OMAP-L137
Hi,
I have two board Using OMAPL_137 chip,I want to boot from nand flash on OMAPl137.However, one board takes more than 30s to boot from flash,while another board takes no more than 1s .By the way ,my two board are not exactly the same in design,and the flash chip is diferrent also.So my question is what cause this differnce?what operation OMAPL137 have to do before boot from nand flash .Does there any datasheet focus on operation before boot?