hi,
recently i use 24bit eeprom as bootloader. However, after i write the bin file to eeprom , the code can not work successfully. but in debug mode the code can work.
here my questions:
1.what is the correct dos command line to create a bin?
2.in the program i use bios , if there is some special requirements about bios bin file (small large or huge)?
3.in debug mode ,i use gel file , but when i delete gel the debug mode cannot work neither. if there is some notes about gel file?
thank you for everyone~