Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAPL138
Hello,
I'm working on the omapl138 board in that I facing the issue in enet_lwip example code when I trying to create a new project root (third_party/lwip-1.3.2/apps/httpserver_raw_io/fsdata_evmAM1808.c) "fs_evmAM1808.c" file it's giving below-mentioned error but when I open a prebuilt path of starter-ware code of enet_lwip it is not giving any error and HTTP code working fine. Please solve this problem I have been facing this issue past two weeks.
Error i'm facing
#28 expression must have a constant value
#71 incomplete type is not allowed
Working : Starterware directory

Error FIle