Hi Experts,
I want to attach interrupt 392(GIC500) to GPIO0_30/AF21, the following is my code,
Please help to check it,
struct tisci_msg_rm_irq_set_req rmIrqReq;
struct tisci_msg_rm_irq_set_resp rmIrqResp;
memset(&rmIrqReq, 0, sizeof(rmIrqReq));
rmIrqReq.valid_params |= TISCI_MSG_VALUE_RM_DST_ID_VALID;
rmIrqReq.valid_params |= TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID;
rmIrqReq.src_id = TISCI_DEV_GPIOMUX_INTRTR0;
rmIrqReq.global_event = 0U;
/*CSLR_WKUP_GPIOMUX_INTRTR0_IN_WKUP_GPIO0_GPIO_BANK_0*/
rmIrqReq.src_index = 103U;/*WKUP_GPIOMUX_INTRTR0_IN_103*/
rmIrqReq.dst_id = TISCI_DEV_COMPUTE_CLUSTER0_GIC500SS;
/*CSLR_COMPUTE_CLUSTER0_GIC500SS_SPI_GPIOMUX_INTRTR0_OUTP_8*/
rmIrqReq.dst_host_irq = 392U;
rmIrqReq.ia_id = 0U;
rmIrqReq.vint = 0U;
rmIrqReq.vint_status_bit_index = 0U;
rmIrqReq.secondary_host = TISCI_MSG_VALUE_RM_UNUSED_SECONDARY_HOST;
printf("setting gic router\n");
if (0 == Sciclient_rmIrqSet(
&rmIrqReq, &rmIrqResp, SCICLIENT_SERVICE_WAIT_FOREVER)) {
printf("Sciclient_rmIrqSet failed\n");
return 1;
}
printf("setting gic router done\n");
Thanks,
Jianqiang