Part Number: TDA4VM
Hi TI,
I want to implement an Interrupt in a FreeRTOS application (PSDK v08.00). I want to use Pulsed Interrupts, since the behaviour of HwiP_irq_handler_c in packages/ti/kernel/freertos/portable/TI_CGT/r5f/port_Hwi.c (line 125-182), cleares Pending Interrupt Bits from Pulsed Interrupts BEFORE execution of ISR and Leveled Interrupt AFTER execution of ISR. In case of Leveled Interrupts, this can lead to a situation, where the Pending Interrupt bit gets cleared, although the upcoming ISR is not yet executed. This will result in a lost interrupt.
To implement the interrupt, I am using HwiP Interface. Unfortunately, I do not see a way to tell VIM, that my Interrupt has to be a Pulsed Interrupt. However, for AM64xx Devices, I found the following Documentation of HwiP Interface: https://software-dl.ti.com/mcu-plus-sdk/esd/AM64X/08_00_00_21/exports/docs/api_guide_am64x/structHwiP__Params.html Here HwiP_Params consists of a data field called "isPulse", which can configure any Interrupt as Pulse or Level Interrupt.
Q1: Are there plans to add this functionality also to J721e PDK? Or is there something similar already included?
In the meantime, I found the following workaround: R5FSS_VIM_INTTYPE_j register (0x0FF8041Ch + (j * 20h)) indicates whether an interrupt is a pulse or level source. This register is also writable. So I manually write 1 to the correct bit of the corresponding register (in case of interrupt idx 256, the corresponding register would be 0x0FF8051C where I write 0x1).
Q2: I this the intended usage of this register? Or are there some side effects when manipulating this register manually?
Thanks for your help and best regards,
Felix