Part Number: AM3354
Hi TI
There's a question that a Customer wants to clarify.
My customer uses AM3354 with PLC via 10/100M RMII interface.
According to them, their PLC device support MII and RMII, But RXER pin of PLC will be used for other purpose.
Please answer to the questions below.
1. Is is possible to communicate via RMII without RXER signal?
2. Original thread said MAC to MAC has not been verified. How about this PLC case? I don't have the information wherther their PLC has MAC and PHY mode.
3. Is it necessary to add Pull Up/Down to RXER pin even the pin is unused. I am confused by original thread. I am not sure the pin should be open-float or pulled down when RMII interface is used without RXER pin.
4. If PU/PD is required when unused, Please suggest the appropriate value.
Regards,
Jack