Part Number: TDA4VM
Hi, experts.
I use vision_apps on TDA4VM.
And I want to implement my application (MCAN) on mcu1_0.
The method is to copy the sample code to "vision_apps \ apps \ basic_demos \ app_rtos \ rtos_linux \ mcu1_0" and then modify and build the code based on this.
Boot this from the SD card with the SBL bootflow.
TI has provided some MCAN samples, which one can I use?
A sample that can work without Autosar is better.
① pdk_jacinto_08_00_00_37 \ packages \ ti \ csl \ example \ mcan \ mcanEvmLoopback \ mcan_evm_loopback_app_main_k3.c
② mcusw \ mcuss_demos \ profiling \ can_profile.c
③ pdk_jacinto_08_00_00_37 \ packages \ ti \ board \ diag \ mcan \ src \ mcan_test.c
■ SDK
ti-processor-sdk-rtos-j721e-evm-08_00_00_12
ti-processor-sdk-linux-j7-evm-08_00_00_08
Regards,