Part Number: TDA4VM
Hi, experts.
I'm running csl_mcan_evm_loopback_app with CCS.
<pdk_jacinto_08_00_00_37\packages\ti\csl\example\mcan\mcanEvmLoopback\mcan_evm_loopback_app_main_k3.c>
When I run it, I got an error on the console. What should I do with this error?
■ Build command
gmake csl_mcan_evm_loopback_app
■ SDK
ti-processor-sdk-rtos-j721e-evm-08_00_00_12
ti-processor-sdk-linux-j7-evm-08_00_00_08
■ Console log
[MCU_Cortex_R5_0] SCICLIENT_CCS_INIT: Jun 15 2021, 16:59:35Sciclient_Init Passed. ================================================================= DEVGRP = 1 ================================================================= SYSFW Common Board Configuration with Debug enabled... PASSED SYSFW PM Board Configuration... PASSED SYSFW Security Board Configuration... PASSED ================================================================= Sciclient Dev Group 01 initilization started Power on the WKUPMCU to MAIN and MAIN to WKUPMCU VDs... PASSED ================================================================= DEVGRP = 2 ================================================================= SYSFW Common Board Configuration with Debug enabled... PASSED SYSFW PM Board Configuration... PASSED SYSFW Security Board Configuration... PASSED ================================================================= DMSC Firmware Version 21.5.0--v2021.05 (Terrific Llam Firmware revision 0x15 ABI revision 3.1 ================================================================= Sciclient_ccs_init Passed. SCISERVER Board Configuration header population... PASSED Starting Application... Available MCAN Module for usage: 0. BA: 0x40500000 - MCU_MCAN0. 1. BA: 0x40540000 - MCU_MCAN1. 2. BA: 0x2728000 - MAIN_MCAN2. Enter MCAN Module to use: 0 MCAN Clock Configuration Successful. MCAN Node Type: 1. Transmitter Side. 2. Receiver Side. 3. Loopback - no external transmission/reception Enter type of the node: 1 SciClient Interrupt Params Configuration passed for offset: 1 SciClient Interrupt Params Configuration passed for offset: 2 Error in SciClient Interrupt Params Configuration!!!offset: 0 CrossBar/Interrupt Configuration failed. MCANSS Revision ID: scheme:0x1 Business Unit:0x2 Module ID:0x8e0 RTL Revision:0x9 Major Revision:0x1 Custom Revision:0x0 Minor Revision:0x1 CAN-FD operation is enabled through E-Fuse. Endianess Value: 0x87654321 Transmitter Side application: This test will send 15 messages with various payload varying from 1byte to 64bytes. Message Object: Message ID: 0x100000 Message Remote Transmission Request: 0x0 Message Extended Frame ID(0:11Bit ID/1:29bit ID): 0x0 Message Error State Indicator(0:Error Active/1:Error Passive): 0x0 Message Data Length Code: 0xf Message BRS: 0x1 Message CAN FD format: 0x1 Message Store Tx Events: 0x1 Message Marker: 0xaa Message DataByte0: 0x0 Message DataByte1: 0x1 Message DataByte2: 0x2 Message DataByte3: 0x3 Message DataByte4: 0x4 Message DataByte5: 0x5 Message DataByte6: 0x6 Message DataByte7: 0x7 Message DataByte8: 0x8 Message DataByte9: 0x9 Message DataByte10: 0xa Message DataByte11: 0xb Message DataByte12: 0xc Message DataByte13: 0xd Message DataByte14: 0xe Message DataByte15: 0xf Message DataByte16: 0x10 Message DataByte17: 0x11 Message DataByte18: 0x12 Message DataByte19: 0x13 Message DataByte20: 0x14 Message DataByte21: 0x15 Message DataByte22: 0x16 Message DataByte23: 0x17 Message DataByte24: 0x18 Message DataByte25: 0x19 Message DataByte26: 0x1a Message DataByte27: 0x1b Message DataByte28: 0x1c Message DataByte29: 0x1d Message DataByte30: 0x1e Message DataByte31: 0x1f Message DataByte32: 0x20 Message DataByte33: 0x21 Message DataByte34: 0x22 Message DataByte35: 0x23 Message DataByte36: 0x24 Message DataByte37: 0x25 Message DataByte38: 0x26 Message DataByte39: 0x27 Message DataByte40: 0x28 Message DataByte41: 0x29 Message DataByte42: 0x2a Message DataByte43: 0x2b Message DataByte44: 0x2c Message DataByte45: 0x2d Message DataByte46: 0x2e Message DataByte47: 0x2f Message DataByte48: 0x30 Message DataByte49: 0x31 Message DataByte50: 0x32 Message DataByte51: 0x33 Message DataByte52: 0x34 Message DataByte53: 0x35 Message DataByte54: 0x36 Message DataByte55: 0x37 Message DataByte56: 0x38 Message DataByte57: 0x39 Message DataByte58: 0x3a Message DataByte59: 0x3b Message DataByte60: 0x3c Message DataByte61: 0x3d Message DataByte62: 0x3e