This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: AM5728:CPTS interrupt don't work

Part Number: AM5728


Dear TI experts:

We use processor_sdk_rtos_am57xx_6_03_00_106 and board idk572x.

We need to process PTP packets using CPTS on A15 core with Gigabit port.

I give below the initialization code CPTS:

int volatile * const control = (int*)0x48484C04;
 *control |= (0 << 0);

 int volatile * const ts_ltype = (int*)0x4848402C;
 *ts_ltype = 0x88F7;

 const uint32_t seqOffset = 0x1E;

 int volatile * const p1_control = (int*)0x48484200;
 *p1_control = (*p1_control & 0xffef0000)|(
 (1 << 0) | // Port 1 Receive Time Sync enableds */
 (1 << 1) | // Time Sync Transmit Enable */
 (1 << 2) | // Time Sync LTYPE 1 enable */
 (1 << 4) | // stamp annex D packets */
 (1 << 5) | // stamp annex E packets */
 (1 << 6) | // stamp annex F packets */
 (1 << 7) | // stamp unicast packets */
 (1 << 8)); // stamp packets with nonzero ttl */

 int volatile * const p1_ts_seq_mytype = (int*)0x4848421C;
 *p1_ts_seq_mytype = (seqOffset << 16) | 0xFFFF;

 int volatile * const cpts_int_en = (int*)0x48484C28;
 *cpts_int_en |= (1 << 0);

 *control |= (1 << 0); /* CPTS_EN */

CSL_xbarMpuIrqConfigure(CSL_XBAR_INST_MPU_IRQ_94, CSL_XBAR_GMAC_SW_IRQ_MISC_PULSE);
 Hwi_construct(&CptsHwiHandler, 94 + 32, CptsHwi, NULL, NULL);

CSL_CPSW_enableWrMiscInt(WrRegs, 0, 16); /* BIT(4) is the CPTS IRQ EN */

We generate test packets using PTPD. Ethernet statistic show receiving packets, but we don't watch interrupts CPTS_EVENT_PACKET_RX in CCS

I present our test project below.

cpts-test.zip

Please tell me where we went wrong and why we do not see interrupt events for receiving packet?

Best Regards,
Alex