Other Parts Discussed in Thread: CCSTUDIO
Hi,
I have got 2 DM6437 (one is transmitter and other Receiver )
Both has been connected to LAN.
With the help of one DM 6437 i captured a video and passed it via LAN , made it as preview in the GUI (Hosp application ) , at the receiver side.
There is no option for the real time utilization of that incoming video, so that i stored it in Hard Disk at the receiver side.
my doubt is, i need to visualize the incoming Video in the screen via DM6437 in the receiver side, in a real time cases.
That is , i need to modify the HOST application (GUI), so that while capturing video at the transmitter side, i need to visualize it in the receiver side , via DM6437 in the two extreme side.
i need to modify GUI or any development in program coding section part ?
Kindly help me !!!!!!!!!!!