This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VPBE with dm437



I have got 2 DM6437 (one is transmitter and other Receiver )

Both has been connected to LAN.

With the help of one DM 6437 i captured a video and passed it via LAN , made it as preview  in the GUI (Hosp application ) , at the receiver side.

There is no option for the real time utilization of that incoming video, so that i stored it in Hard Disk at the receiver side.

 my doubt is, i need to visualize the incoming Video in the screen via DM6437 in the receiver side, in a real time cases.

That is , i need to modify the HOST application (GUI), so that  while capturing video at the transmitter side, i need to visualize it in the receiver side , via DM6437 in the two extreme side.

For this whether VPBE drivers play any role ?