Make install for the SDcard is not working.
Command issued:
- export PATH="/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/linux-devkit/sysroots/x86_64-arago-linux/usr/bin:$PATH"
- GCC92PATH=/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/linux-devkit/sysroots/x86_64-arago-linux/usr/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/bin/:/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/linux-devkit/sysroots/x86_64-arago-linux/usr/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/bin/:
- export PATH=$GCC92PATH:$PATH
- cd ~/ti-processor-sdk-linux-j7-evm-08_00_00_08/
- make
- make install (passed)
- sudo DESTDIR=/media/$USER/rootfs make install (failed)
- sudo cp board-support/u-boot_build/a72/u-boot.img board-support/u-boot_build/a72/tispl.bin board-support/u-boot_build/r5/tiboot3.bin /media/$USER/boot
Link Followed:
1.3. Simplified SDK Build using Top-Level Makefile — Processor SDK Linux for J721e Documentation
===================================
uic68347@igv6350u:~$ df -h
Filesystem Size Used Avail Use% Mounted on
udev 1.2G 0 1.2G 0% /dev
tmpfs 248M 3.3M 245M 2% /run
/dev/mapper/vgroot-root 49G 5.8G 41G 13% /
tmpfs 1.3G 172K 1.3G 1% /dev/shm
tmpfs 5.0M 4.0K 5.0M 1% /run/lock
tmpfs 1.3G 0 1.3G 0% /sys/fs/cgroup
/dev/mapper/vgroot-home 237G 13G 214G 6% /home
/dev/sda3 946M 91M 790M 11% /boot
/dev/sda2 571M 4.4M 567M 1% /boot/efi
tmpfs 248M 12K 248M 1% /run/user/125
tmpfs 248M 28K 248M 1% /run/user/500239492
/dev/sr0 75M 75M 0 100% /media/uic68347/ISOIMAGE
/dev/sdb2 28G 47M 26G 1% /media/uic68347/boot
/dev/sdb1 28G 45M 26G 1% /media/uic68347/rootfs
=================================================================
uic68347@igv6350u:~$ sudo fdisk -l
Disk /dev/sda: 300 GiB, 322122547200 bytes, 629145600 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: gpt
Disk identifier: 171B895C-FC83-44C5-91D3-DBFDCCBA99EE
Device Start End Sectors Size Type
/dev/sda1 2048 4095 2048 1M BIOS boot
/dev/sda2 4096 1175551 1171456 572M EFI System
/dev/sda3 1175552 3176447 2000896 977M Linux filesystem
/dev/sda4 3176448 629143551 625967104 298.5G Linux LVM
Disk /dev/mapper/vgroot-root: 50 GiB, 53653536768 bytes, 104792064 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk /dev/mapper/vgroot-swap: 4 GiB, 4294967296 bytes, 8388608 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk /dev/mapper/vgroot-home: 240 GiB, 257698037760 bytes, 503316480 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk /dev/sdb: 55.7 GiB, 59793997824 bytes, 116785152 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: dos
Disk identifier: 0xddddf4b6
Device Boot Start End Sectors Size Id Type
/dev/sdb1 2048 58585087 58583040 28G 83 Linux
/dev/sdb2 58585088 116785151 58200064 27.8G 83 Linux
===========================================================================
INSTALL sound/usb/snd-usbmidi-lib.ko
DEPMOD 5.10.41-g4c2eade9f7
make[1]: Leaving directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/board-support/linux-5.10.41+gitAUTOINC+4c2eade9f7-g4c2eade9f7'
==============================================
Installing ARM Benchmarks - Release version
==============================================
make[1]: Entering directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/arm-benchmarks-1.3'
for dir in dhrystone whetstone linpack; do \
make -C $dir install; \
done
make[2]: Entering directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/arm-benchmarks-1.3/dhrystone'
dhrystone release version installed.
make[2]: Leaving directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/arm-benchmarks-1.3/dhrystone'
make[2]: Entering directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/arm-benchmarks-1.3/whetstone'
whetstone release version installed.
make[2]: Leaving directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/arm-benchmarks-1.3/whetstone'
make[2]: Entering directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/arm-benchmarks-1.3/linpack'
linpack release version installed.
make[2]: Leaving directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/arm-benchmarks-1.3/linpack'
make[1]: Leaving directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/arm-benchmarks-1.3'
===============================================
Installing AM Sysinfo - Release version
===============================================
make[1]: Entering directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/am-sysinfo-git'
for dir in mem_util; do \
make -C $dir install; \
done
make[2]: Entering directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/am-sysinfo-git/mem_util'
mem_util release version installed.
make[2]: Leaving directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/am-sysinfo-git/mem_util'
make[1]: Leaving directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/am-sysinfo-git'
=============================================
Installing OProfile Example - Debug version
=============================================
make[1]: Entering directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/oprofile-example'
oprofile_example optimized debug version installed.
oprofile_example debug version installed.
make[1]: Leaving directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/example-applications/oprofile-example'
================================
Installing cryptodev-linux
================================
make[1]: Entering directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/board-support/extra-drivers/cryptodev-module-1.10'
make -C /home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/board-support/linux-5.10.41+gitAUTOINC+4c2eade9f7-g4c2eade9f7 M=/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/board-support/extra-drivers/cryptodev-module-1.10 ARCH=arm64 CROSS_COMPILE=/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/aarch64-none-linux-gnu- modules_install
make[2]: Entering directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/board-support/linux-5.10.41+gitAUTOINC+4c2eade9f7-g4c2eade9f7'
INSTALL /home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/board-support/extra-drivers/cryptodev-module-1.10/cryptodev.ko
DEPMOD 5.10.41-g4c2eade9f7
make[2]: Leaving directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/board-support/linux-5.10.41+gitAUTOINC+4c2eade9f7-g4c2eade9f7'
make[1]: Leaving directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/board-support/extra-drivers/cryptodev-module-1.10'
=============================
Installing SYSFW Image
=============================
Nothing to do
====================================
Installing ti-img-rogue-driver
====================================
make[1]: Entering directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/board-support/linux-5.10.41+gitAUTOINC+4c2eade9f7-g4c2eade9f7'
INSTALL /home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/board-support/extra-drivers/ti-img-rogue-driver-1.13.5776728/binary_j721e_linux_wayland_release/target_aarch64/kbuild/pvrsrvkm.ko
DEPMOD 5.10.41-g4c2eade9f7
make[1]: Leaving directory '/home/uic68347/ti-processor-sdk-linux-j7-evm-08_00_00_08/board-support/linux-5.10.41+gitAUTOINC+4c2eade9f7-g4c2eade9f7'
=============================
Updating oob-demo wallpaper
=============================
sed -i 's%background-image.*%background-image=/usr/share/demo/j7-evm-p0-wallpaper.jpg%' /media/uic68347/rootfs/etc/weston.ini
sed: can't read /media/uic68347/rootfs/etc/weston.ini: No such file or directory
Makefile:258: recipe for target 'oob-demo_install' failed
make: *** [oob-demo_install] Error 2
uic68347@igv6350u:~/ti-processor-sdk-linux-j7-evm-08_00_00_08$
Also noticed there is no /etc folder created in the /rootfs partition