Part Number: TDA4VM
Other Parts Discussed in Thread: DRA829V
Hi experts
I have download the
| ti-processor-sdk-linux-sk-tda4vm-etcher-image.zip |
and burn it in SanDisk 16GB SD card
But when I start the board, the error occured
U-Boot SPL 2021.01-g53e79d0e89 (Sep 02 2021 - 18:20:00 +0000) Model: Texas Instruments K3 J721E SoC Board: J721EX-PM2-SOM rev E8 SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam') Trying to boot from MMC2 spl_load_image_fat: error reading image tispl.bin, err - -6 spl_load_image_ext: ext4fs mount err - 0 SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ###
And I need to restart a number of times to load, the following error is reported every time
I think it is a hardware issue
Have you encountered this problem, and how do you solve it?