Other Parts Discussed in Thread: CCSTUDIO
Dear Ti members,
I am using DSK 6713. I want to use HPI port for digital output. I want to send data at certain time interval irrespective of the address signal, handshaking signals,interrupt signal. In a word I want to use it as a GPIO as paralel output of digital data at a certain interval, which will be controled by program.
I have gone through the the example loacted at C:\CCStudio_v3.1\examples\dsk6713\rtdx, but did not understand whether it is for HPI port or for something else.
If is for HPI port then I am not understanding how to modify the code for the above memtioned purpose. I am giving the code of that example.
I expect your kind help.
CODE:
/*************************************************************************
* FILENAME: $RCSfile: t2h.c,v $
* VERSION : $Revision: 1.1 $
* DATE : $Date: 2000/11/03 19:12:05 $
* Copyright (c) 1997-2000 Texas Instruments Incorporated
*
* Target-To-Host Test:
*____________________________________________________________________
* - Sends 100 integers, one at a time via RTDX_write().
* - Uses ONE output channel.
*
* - Tests Data transmission from target to host at the User layer.
* - This is the module to be run on the TARGET.
* - This program is meant to be used with the RTDX Diagnostics
* Control's Target-To-Host test option.
*************************************************************************/
#include <stdio.h> /* fprintf(), puts() */
#include <stdlib.h> /* abort() */
#include <rtdx.h> /* RTDX */
#include "target.h" /* TARGET_INITIALIZE() */
/* Declare and initialize an output channel called "ochan" */
RTDX_CreateOutputChannel(ochan);
#define NUMBER_MESSAGES 100
void main( void )
{
unsigned int data;
/* Target Specific Initialization */
TARGET_INITIALIZE();
/* Enable the output channel, "ochan" */
RTDX_enableOutput(&ochan);
printf("Sending %d Messages to Host...\n", NUMBER_MESSAGES);
for ( data = 0; data < NUMBER_MESSAGES; data++ )
{
/* Send the data to the host */
if ( !RTDX_write( &ochan, &data, sizeof(data) ) )
{
fprintf(stderr, "\nError: RTDX_write() failed!\n");
abort();
}
/* Wait for Target-to-Host transfer to complete */
while ( RTDX_writing != NULL )
{
#if RTDX_POLLING_IMPLEMENTATION
/* If polling implementation of RTDX... */
/* ...call RTDX_Poll to do data transfer */
RTDX_Poll();
#endif
}
/* Display what was sent in the stdout window */
fprintf(stdout, "Value %i was sent to the host\n", data);
}
/* Disable the output channel, "ochan" */
RTDX_disableOutput(&ochan);
puts("\nTest Completed!");
}
Thanking you
Regards
Biprangshu Saha