I want to connect the much maximum 1 bit ECC nand Flash to DM/AM37XX ,how much maximum can I select the NAND FLASH.
If I designed a PDA use the DM3730 in WINCE ,if I need to buy a xds560 emulator .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have info about memory selection here:
http://processors.wiki.ti.com/index.php/Memory_Vendor_Selection_Guide
I will check about the emulator question.
Regards,
Michael T
I design a product with the AM3715 ,Beacuse there is little 1 bit ECC nand flash,some 1 bit ECC flash would able to stop production. So I want to use a BGA eMMC to storage the program and data ; and what to I can flash the program into the eMMC ,when the POS products dive into product line in the factory.
Now the POS product has a NAND flash and eMMC,
and so later I would design the product only use the eMMC ,don not use the NAND flash.