Part Number: 66AK2H12
Hi Expert,
My customer found a issue that one L1P cache line value (marked as red in below pictures)can not automatically sync up L2 memory value of function(Timer64_Init). The dirty bit in cache status is "0". The result will cause system crash.
The L2 memory value is 0x021FECA3 0x019839A0
The L1P cache line value is 0x0006CF10 0x00008000

The issue only occurred when the function (Timer64_Init) located in a special memory address(0x17877FF0).
If customer changed the function code memory map from 0x17877FF0 to 0x17878000, the issue disappeared,
or make a cache L1P all invalid before the function call, the issue also disappeared. Issue disappeared means that the L1P cache line value can sync up the L2 memory and running successfully.
Customer push for the root-cause on this issue, could you help it?