Hello Everyone,
I have been facing DSS init problems related to DPI interface while trying to boot a Mistral OMAP3 EVM board using kernel 2.6.35.11 (from mainline). Due to the DPI error, omapfb cannot be probed and no displays are available.
After getting kernel sources, setting "omap3_evm_defconfig", crosscompiling the sources and bootting, I have:
Linux version 2.6.35.11 (fernando@dhws063) (gcc version 4.5.1 (Sourcery G++ Lite 2010.09-50) ) #37 Tue Apr 12 13:10:00 BRT 2011
CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
Machine: OMAP3 EVM
Memory policy: ECC disabled, Data cache writeback
OMAP3430/3530 ES3.1 (l2cache iva sgx neon isp )
SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x100000
Reserving 4194304 bytes SDRAM for VRAM
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
Kernel command line: mem=256M console=ttyS0,115200n8 ip=dhcp root=/dev/nfs nfsroot=/home/tux/nfs/angstrom1,nolock noinitrd rw
... ... ... ... ...
... ... ... ... ...
OMAP DSS rev 2.0
omapdss DPI error: can't get VDDS_DSI regulator
omapdss CORE error: Failed to initialize dpi
... ... ... ... ...
... ... ... ... ...
omapfb omapfb: failed to setup omapfb
omapfb: probe of omapfb failed with error -22
regulator_init_complete: incomplete constraints, leaving VDVI on
... ... ... ... ...
... ... ... ... ...
Freeing init memory: 156K