Use IMX390 + ub953 camera driver, with SDK7.0 version, run the single camera demo, using 7.0 edition, point code doesn't change, and the situation now is blocked vxGraphParameterDequeueDoneRef this program.
VxGraphParameterDequeueDoneRef above three vxGraphParameterEnqueueReadyRef were successful, but to have a problem, the queue when I in front of the vxGraphParameterDequeueDoneRef added
VxGraphParameterCheckDoneRef function, after the log found num_refs_capture returns 0, no content can be out of the queue.
How to solve this problem?