This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6548: AM6548 Docker image is cracked (SDK8.0)

Part Number: AM6548

Hi.

When using the Docker image to boot AM6548 GP EVM, you just need to do "grep" some words in the root dir.

It will show "EL3" and this is serious kernel panic.

How to solve this?

BR Rio

root@am64xx-evm:/# grep -r "docker.io" .
Unhandled Exception in EL3.
x30 = 0x00000000701a0e6c
x0 = 0xffff8000125a000c
x1 = 0x000000000000000c
x2 = 0xffff800010685070
x3 = 0xffff800010685210
x4 = 0x0000000000000000
x5 = 0x00000000fffffff7
x6 = 0xffff000029434037
x7 = 0x000000000000000f
x8 = 0xffff00003d5b2f80
x9 = 0x0000000000000000
x10 = 0x0000000000000000
x11 = 0x0000000000000000
x12 = 0xffff000029434030
x13 = 0xffff000029436000
x14 = 0x0000000000000005
x15 = 0xffff00003ba32f30
x16 = 0x0000000000000000
x17 = 0x0000000000000000
x18 = 0x0000000000000020
x19 = 0xffff0000260e3080
x20 = 0x000000000000000c
x21 = 0xffff80001a54fd4c
x22 = 0xffff80001a54fd4c
x23 = 0x0000000000002000
x24 = 0xffff80001a54fe30
x25 = 0x000000000001fffc
x26 = 0x0000000000000001
x27 = 0xffff800010dc96c8
x28 = 0xffff000024dd7000
x29 = 0xffff80001a54fc10
scr_el3 = 0x000000000000073d
sctlr_el3 = 0x0000000030cd183f
cptr_el3 = 0x0000000000000000
tcr_el3 = 0x0000000080803520
daif = 0x00000000000002c0
mair_el3 = 0x00000000004404ff
spsr_el3 = 0x0000000020000085
elr_el3 = 0xffff80001068507c
ttbr0_el3 = 0x00000000701ad780
esr_el3 = 0x0000000092000010
far_el3 = 0xffff8000125a000c
spsr_el1 = 0x0000000020000005
elr_el1 = 0xffff800010a7736c
spsr_abt = 0x0000000000000000
spsr_und = 0x0000000000000000
spsr_irq = 0x0000000000000000
spsr_fiq = 0x0000000000000000
sctlr_el1 = 0x0000000034d4d91d
actlr_el1 = 0x0000000000000000
cpacr_el1 = 0x0000000000300000
csselr_el1 = 0x0000000000000000
sp_el1 = 0xffff80001a54fc10
esr_el1 = 0x0000000056000000
ttbr0_el1 = 0x00000000a6065200
ttbr1_el1 = 0x0bac000082f10000
mair_el1 = 0x000c0400bb44ffff
amair_el1 = 0x0000000000000000
tcr_el1 = 0x00000032f5d07590
tpidr_el1 = 0xffff80006ed50000
tpidr_el0 = 0x0000ffff922b36b0
tpidrro_el0 = 0x0000000000000000
par_el1 = 0x0000000000000000
mpidr_el1 = 0x0000000080000001
afsr0_el1 = 0x0000000000000000
afsr1_el1 = 0x0000000000000000
contextidr_el1 = 0x0000000000000000
vbar_el1 = 0xffff800010010800
cntp_ctl_el0 = 0x0000000000000005
cntp_cval_el0 = 0x0000000db02bf4c5
cntv_ctl_el0 = 0x0000000000000000
cntv_cval_el0 = 0x0000000000000000
cntkctl_el1 = 0x00000000000000d6
sp_el0 = 0xffff00003ba32a00
isr_el1 = 0x0000000000000040
dacr32_el2 = 0x0000000000000000
ifsr32_el2 = 0x0000000000000000
cpuectlr_el1 = 0x0000000000000040
cpumerrsr_el1 = 0x0000000008100303
l2merrsr_el1 = 0x0000000013107708
cpuactlr_el1 = 0x00001000090ca000

  • Hi .

    I found we cannot perform any "grep" cmd under the root path.

    And no matter you try to grep something on the root path, this issue will be reproduced on the TI EVM.

    please help to solve if any.

    BR Rio

  • Rio,

    That is indeed strange. I tried on DRA821-EVM & it does not crash. 

    root@j7200-evm:/# grep -r "docker.io" .
    grep: ./lib/modules/5.10.41-g4c2eade9f7/source: No such file or directory
    grep: ./lib/modules/5.10.41-g4c2eade9f7/build: No such file or directory
    grep: ./lib/modules_bk/5.10.41-g4c2eade9f7/source: No such file or directory
    grep: ./lib/modules_bk/5.10.41-g4c2eade9f7/build: No such file or directory
    grep: ./lib/modules_bk1/5.10.41-g4c2eade9f7/source: No such file or directory
    grep: ./lib/modules_bk1/5.10.41-g4c2eade9f7/build: No such file or directory

    root@am64xx-evm:/# grep -r "docker.io" .

    One strange thing. Why is it called AM64xx? It should be AM65xx. Do you have a special file system of you own?

    - Keerthy

  • Hi Keerthy:

    I found this syndrome by using SDK8.0.

    The kernel will be crushed "ONLY" if you perform the "Grep cmd" in the root path.

    If you perform the "Grep cmd" in the sub dir, the kernel will not crush.

    I think the docker developer shall fix it.

    BR Rio

  • Hi Rio,

    The support for docker on the AM6548 was experimental in nature and not fully tested/validated. It is not to be used.

    We will fix the documentation for the next release.

    Regards

    Karthik