This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GUI with DM6437

Hi,

I am practicing with GUI incorporate dm6437.

On the host application side, i detected the target and received a video from target board(DM6437).

Now i am intended to view the video in screen via DM6437 at the host side.

Whether i need to do anything with VPBE driver ?

pls help me

  •  

    If the DM6437 has to display the received image, on the screen, Yes - you will have to use th VPBE drivers, to output the image to the screen.

    Hope this helps.

  • Sir,

    My real problem is:

    I have got 2 DM6437 (one is transmitter and other Receiver )

    Both has been connected to LAN.

    With the help of one DM 6437 i captured a video and passed it via LAN , made it as preview  in the GUI (Hosp application ) , at the receiver side.

    There is no option for the real time utilization of that incoming video, so that i stored it in Hard Disk at the receiver side.

     my doubt is, i need to visualize the incoming Video in the screen via DM6437 in the receiver side, in a real time cases.

    That is , i need to modify the HOST application (GUI), so that  while capturing video at the transmitter side, i need to visualize it in the receiver side , via DM6437 in the two extreme side.

    Now,  tell me, whether  i need to do with VPBE only ?