Other Parts Discussed in Thread: DM3730
Here is the specific questions regarding CODEC performance on the 1GHz DM3730 processor
1) In addition to H.264 encoding, can the DSP, or possibly PowerVR SGX also perform scaling of the video as well. This would be prior to encoding and not a scaling on playback operation. Not temporal scaling but resolution scaling, i.e. upscaling from 480p to 720p.
2) Can the CODEC also perform motion adaptive de-interlacing of NTSC/PAL signals once they are decoded. If not motion adapting, can it perform some level of blending or field extension deinterlacing? Can any of these operations be performed in the PowerVR SGX prior to sending to CODEC for encoding.
The person answering may have some questions WRT bit rate of the encoding. If so, just let us know what the limitations are. I’m supposed to have a call with this customer tomorrow and really would like to know the scaling question.
-Tom-