This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Graphics Controller Selection

Dear TI Support,

We are in the process of selecting the Graphics controller chip which is substitute to MB86298 Fujitsu graphics controller. Our previous design was based on MB86298 and are looking at options to migrate to TI device. Our application has 2 analog RGB STANAG 3350B inputs which would be digitized and given to graphics controller for graphics symbol over laying function. Over layed video output will be sent out from board in analog STANAG RGB format only. Graphics controller can provide digital RGB or YCbCr data which can be converted to analog RGB using separate decoders. Host Processor will talk to this Graphics controller on PCIe Gen-1. Graphics controller should support OpenGL ES 2.0 symbology control from Host Processor. 2 Video inputs and outputs should be processed simultaneously with overlaying.

Regards,

Erfan

  • Hello Erfan,

    Thank you for your post and sorry for the delay. Since there are so many factors involved in making this decision, may I request that you reach out to your business contact to set up a discussion on this topic? I would like to understand the goals to be able to make any recommendations. Please do refer to this e2e thread and my request so that we can take this forward.

    Regards

    Hemant