Part Number: PROCESSOR-SDK-OMAPL138
Other Parts Discussed in Thread: OMAPL138
Hello
I want to run CSL examples present in pdk folder on OMAP L138 LCDK. I have started using GPIO Module present in path "C:\ti\pdk_omapl138_1_0_11\packages\ti\csl\example\gpio".
I have added relevant C source files and header files from folder "C:\ti\pdk_omapl138_1_0_11\packages\ti\csl\src\ip\gpio" as well as interrupt files from path "C:\ti\pdk_omapl138_1_0_11\packages\ti\csl\src\intc".
But I am facing error for the functions stated below:
"_CSL_intcCpuIntrTable " ./_csl_intcIsrDispatch.obj
"__c_int00 " ./_csl_intcIsrDispatch.obj
The error says "unresolved symbol __c_int00, first referenced in ./_csl_intcIsrDispatch.obj gpio_csl C/C++ Problem"
for both functions.
Though I have the functions declaration and definitions of the functions in my C source files. but still it is not picking up.
Kindly let me know how can I be able to run csl examples that include interrupts as well.
If you have any CSL based working code of C6748 with interrupts then please do share.