Hello,
I've been having problems in installing C6RUN , I have followed the Standalone setup on the Getting started wiki, I'm able to config the beagleboard-xM platform using make beagleboard-xM _config , but when I do make dsp_libs it gives me errors signaling that some header files are not present in the /C6run<version>/build/ directory, so I download the missing header files and put them in th required folder, then the make dsp_libs continues and gives errors signaling more missing header and so on! I gave up, as some header files gave error inside them like the one found in include/time.h ! I think what I'm doing is not the correct way, and that these header files should be present from the start?
For a month now I'm not able to fix this, Plz help, I have a grad. project that needs ARM-DSP communication, and C6RUN will help alot!
Thx