This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCIe demo on TDA4VM

the mode of pcie backplane

modprobe netdev

create 6 netport

eth1: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 65510  metric 1
        inet6 fe80::4c18:6bff:fe4d:498d  prefixlen 64  scopeid 0x20<link>
        ether 4e:18:6b:4d:49:8d  txqueuelen 1000  (Ethernet)
        RX packets 160  bytes 46615 (45.5 KiB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 160  bytes 46615 (45.5 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

eth2: flags=4099<UP,BROADCAST,MULTICAST>  mtu 65510  metric 1
        ether 66:0d:bf:3e:41:2e  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 0  bytes 0 (0.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

eth3: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 65510  metric 1
        inet6 fe80::1800:c9ff:fe24:e3e  prefixlen 64  scopeid 0x20<link>
        ether 1a:00:c9:24:0e:3e  txqueuelen 1000  (Ethernet)
        RX packets 162  bytes 46795 (45.6 KiB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 10  bytes 1294 (1.2 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

eth4: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 65510  metric 1
        inet 192.168.2.10  netmask 255.255.255.0  broadcast 192.168.2.255
        inet6 fe80::a06f:6dff:fefe:2bc4  prefixlen 64  scopeid 0x20<link>
        ether a2:6f:6d:fe:2b:c4  txqueuelen 1000  (Ethernet)
        RX packets 177  bytes 48852 (47.7 KiB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 175  bytes 48672 (47.5 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

eth5: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 65510  metric 1
        inet 192.168.1.10  netmask 255.255.255.0  broadcast 192.168.1.255
        inet6 fe80::3c0b:93ff:feed:6fb9  prefixlen 64  scopeid 0x20<link>
        ether 3e:0b:93:ed:6f:b9  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 10  bytes 1271 (1.2 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

eth6: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 65510  metric 1
        inet6 fe80::6013:a9ff:fef1:2e0a  prefixlen 64  scopeid 0x20<link>
        ether 62:13:a9:f1:2e:0a  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 10  bytes 1314 (1.2 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

but eth2  eth5 eth6  are link down.