This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM-Q1: Is there some INT PIN about the TDA4 or just can use the GPIO to accepts interrupt signals

Part Number: TDA4VM-Q1


HI,

1.when PMIC monitors a voltage exceed the limit value , the PMIC will send a INT signal to TDA4 ,is there INT pin at TDA4 ? or I just can connect the PMIC INT signal to a normal GPIO ,and then use the application software to deal this error  ?

2.the PMIC monitor voltage ,Is it written into PMIC by tda4 through I2C? or It is decided by PMIC PDN ? or other way ,I just want to know ,who defined this limit ,and where will this limit range  put in.?

many thanks

BR