This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01022: VDD_WAKE0 power pin connection

Part Number: TIDEP-01022
Other Parts Discussed in Thread: DRA821

Champs,

On the reference design the VDD_WAKE0 power pin is powered by a separate LDO that is switched by the PMIC. (VDD_WK_0V8).  Why is it connected to a switched and enabled LDO?

Is it OK to leave the LDO out and connect it to the Core 0.8V supply?  The power up sequence in the DRA821 DS Fig8-3 shows it coming up at T2 along with other 0.8V volt supplies including Core 0V8.   The datasheet also shows it combined on table 10-1 with the Digital Low Voltage box

The design is not using any low power modes and will always start from a cold start.

thanks

Michael