Dear forum:
Reading Omap-L138 data sheet (SLVSAQ9 of 1/2011 SMOMAP-L138B) I found in JTAG section (page274) - TRST# input has a pull-down resistor and is always asserted during Power-up.
That means that RESET# signal applied to Omap-L138 RESET input (pin-K14) will always cause POWER-ON reset (because TRST- pin-L17 is already=low due to internal pull-down). Is this true?
To implement "warm RESET" - TRST must be in HIGH state. (DS - RESET section page84).
I can make some simple logic (if I want to implement "Warm reset") to bring TRST (L17) to the HIGH state during RESET (K14) input is low.
Will this be sufficient? Or TRST must be = HIGH up to the end of RESETOUT (to have "warm reset")?
There is a diagram for the "warm reset" in DS page86 (Figure 5-5).
But on this diagram TRST stays HIGH all the time and there is no timing shown when TRST must be brought HIGH and then released back to LOW to implement "Warm RESET".
Can somebody provide this information?
Thank you,
Boris Ruvinsky
802-877-4978