Hi All,
I would like to confirm the speed of a DSP chip which I have just bought from an ebay-like site.

Does the number "4" (blurred in the picture) on its upper-right corner indicate it is a 400MHz device?
And does all DM6437 chips have such indicator? I have a EVM which has a 700MHz DM6437 chip on that, but I cannot find a similar numerical indicator "7" like the one above. So does TI always put such number on the upper-right corner?
Sincerely,
Zheng