This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mDDR Low Power Mode

Hi,

I'm a bit confused regarding the DDR controller registers.

Register: SDRCR
Field: LPMODEN

sprugj4b p.49 :

LPMODEN = 1 -> Low Power Mode Enable
LPMODEN = 0 -> Low Power Mode Disable

the defines in the CSLR (cslr_ddr2_mddr.h) are:

#define CSL_DDR2_MDDR_SDRCR_LPMODEN_LPMODE  (0x00000000u)
#define CSL_DDR2_MDDR_SDRCR_LPMODEN_NO_LPMODE (0x00000001u)

Now my questions:

1) Which one is correct?
3) Is it correct, that the SDRAM refreshs/holds data while in low power mode, but can not be read from or written to?
2) Why do I have to set the bit (enable or disable?) the low power mode to do a SyncReset?

Thanks,
Stefan