Hello,
I'm trying to access the GPMC0 peripheral in uboot (3B00 0000h to 3B00 037Ch) but the system crashes on read or writes. Is this caused by the firewall? if yes, how can I enable accessing this memory zone from the A53s?
Details are below:
SDK version is: 8.0.0.21
EVM used: SK-AM64
Modification to show the problem: in uboot file /borad/ti/am64x/evm.c:
Log / Crash dump: