This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J6EVM5777: Boot Up

Part Number: J6EVM5777


It turns out that I had the wrong OTP for the PMIC TPS659039. After replacing OTP 0x85 with OTP 0x87, I now have all the correct voltage outputs.

Here is where we are now.

We have developed a project on J6EVM5777 board using third-party software. Everything works great on J6EVM5777.

We have designed and built a custom DSP board on DRA756BPGABCQ1. The custom board follows the reference design of J6EVM5777, with unnecessary components omitted and a number of ADC chips added.

The board powers up, but SBL fails to load AppImage (see the log below).

The AppImage file is present and does begin with MSTR.

The MLO we use currently was bundled with third-party software.

The SDK we are using is

ti-processor-sdk-rtos-automotive-dra7xx-evm-04.03.00.05-Windows-x86-Install.exe

It has SBL source, but it is unclear how to build MLO for our board because it is based on DRA756BPGABCQ1, and build configurations seem to be provided for various EVM boards.

Any help would be appreciated.

Thanks, Kevin

 DRA75x SBL Boot

 SBL Initial Config Failed

 DPLL Configuration Completed

 Clock Domain Configuration Completed

 Module Enable Configuration Completed

 TI EVM PAD Config Completed
ERROR: HW-Leveling time-out

 DDR Config Completed

 App Image Download Begins

 SD Boot - file open completed successfully

Trying to boot App Image with header version 1
Invalid Magic String in Boot Image
Invalid Magic String in Boot Image
Invalid Magic String in Boot Image
Invalid Magic String in Boot Image

 App Image Download Completed

 Putting MPU CPU1 in Off mode

 EVE MMU configuration completed