Other Parts Discussed in Thread: OMAPL138
What API do i need to use to put the ethernet interface in promiscousmode?
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAPL138
What API do i need to use to put the ethernet interface in promiscousmode?
thank you
Are you asking about C64x? Assuming so, you can install the MCSDK and in the csl you will find an EMAC_setReceiveFilter function in csl_emac.c. There is also a example for using this call, Emac_local_loopback_example.c.
Hope that helps.
We are using the C6748 SOM.
With the software that we installed so far, the function is in the OMAPL-138 source codes (nsp_1_00_00_09\packages\ti\drv\omapl138\ csl_emac.c and ethdriver.c). The string does not appear in any other c code source file in the tree.
The ndk examples run on our hardware, but does that mean that the OMAPL-138 code is being used for the C6748? Do we need to install something else?
Is there a high level document for the calls in this part of the API?
With these calls could i dispense with the network start etc?
Does this levle in the API still give me interrupt handling without having to explicitly program it?
I appreciate that there is an example for the c64, but does that apply to the c6748?
Is there a document that answers these questions directly?
Thank you