Part Number: TMDS64GPEVM
i am trying to boot from the emmc using the reference image provided with SDK 8 but i see no output on the tty port when i set the DIP switch SW2.4 to ON as given in AM64x/AM243x GP EVM User`s guide and everything else is set to default values .
i have flashed the emmc with the same reference image that i use for SD card .
Please note : that i am a load kernel and device tree from emmc by setting the uboot argument mmcdev=0 [emmc] from the sdcard image which means image is perfectly flashed on emmc.
Am i missing something ?
Do i need to recompile the bootloaders/uboot for emmc ?
what uboot argument that i need to set to mount/load rootfs form emmc instead of sdcard ?