This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Network data transfer rate is low

Part Number: TDA4VM

Hi,

I use  Processor SDK RTOS 8.0.0(QNX+RTOS).

I Connected a PHY(LAN8770 RMII mode) to CPSW9G port 4.

Iperf test results are as follows:

UDP :

     External PC  -------->       TDA4           data rate is 93mbps

     TDA4           -------->    External PC     data rate is  11mbps just

TCP:

    The result is similar to that of UDP.

What are the possible causes?

BRs

jeff

 

  • Hi Jeff,

    What exact command are you using for iperf3?

    Who is server and who is client?

    Please provide wireshark traces for the exchange?

    Also can you please confirm that you are not using any filters.

    Moreover, to debug this, you can see the ethernet statistics by running gel files in CCS. See this link for more details on the same. The path for the gel files in sdk is - "[RTOS-SDK-INSTALL-DIR]//pdk_jacinto_08_00_00_37/packages/ti/drv/enet/tools/debug_gels/cpsw_startup.gel"

    Regards,

    Tanmay