Other Parts Discussed in Thread: OMAPL138, OMAP-L138, OMAP-L137
Hi,
We have right now a dsp application running on a C6748 in a battery powered handset
We are considering a pure tactile solution (smartphone like) for our new hmi.
can you tell me which processor family, if any, would be the best suited for that purpose?
We assume the best choice should be a dual (or more) core, one running android (arm I suppose) an the other (dsp) running our application.
Characteristics&constraints:
- Dsp current application runs on our propoer (very light) OS, but could be ported under RT-OS (or android) if necessary
- current Dsp application load: ~50% @375MHz
- Low power oriented (battery powered)
- Android processor should be powerfull enough for a quick response and fluent hmi apperance
- We have already considered the omapL138 but i wonder if the arm9 running at around 400MHz is good enough, furthermore it does not have any graphical coprocessor...
Thanks,
Bruno