This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5504 versus C5505

Other Parts Discussed in Thread: TMS320C5504, TMS320C5505

 

Hi All,

I have a PCB that is completed and working, with schematic drawn for C5505, but actually running with the C5504 part.  Are there *ANY* differences in pin configuration that I need to be aware of?

Secondly, (and one of the issues I'm concerned about), I want to use pins D10, A11, B11, C11 ADC inputs, but on the C5504 spec, they are RESERVED (didn't realize that while drawing the schematic).  On the C5505, they are valid ADC inputs.  Is it OK to have have resistors pulling the ADC inputs up/down on the current C5504 design?

It looks like there may be other small differences, (other than the LCD interface, memory size, and FFT-co), but does it matter?

Thanks...