Part Number: PROCESSOR-SDK-AM64X
I plan to implement a platform based on AM64x, which should be able to work with OPC UA over TSN. According to the reference manual, full TSN support is only available on PRU-ICSSG, but I did not find this feature in the current SDK, checking TSN on PRU-ICSSG. Maybe I didn't look carefully, are there examples in the PRU-ICSSG SDK for TSN? Do I understand correctly that the current TSN support for CPSW is limited only to the subject of the standards that are in the reference manual, and not a complete set of TSN standards on CPSW is supported? If we would like to use a full TSN, should we do on PRU-ICSSG?