Hi Team,
Are there pre-programmed unique MAC addresses available for the two CPSW Ethernet porst?
The TRM mentions CTRLMMR_MAC_ID0 and CTRLMMR_MAC_ID1. Are these used for one of the ports?
Thanks,
Robert
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Are there pre-programmed unique MAC addresses available for the two CPSW Ethernet porst?
The TRM mentions CTRLMMR_MAC_ID0 and CTRLMMR_MAC_ID1. Are these used for one of the ports?
Thanks,
Robert
Robert,
The devices are provided by TI pre-programmed with GUIDs for the MAC ports. Please note that MAC_ID0 and MAC_ID1 define a range of addresses as this device has 3 ports (one internal (P0) and two external (P1 & P2)). ID0 is the address of P0 and ID1 is the address of P2. The address for P1 is the value between them.
Hope this helps