Hi
I wonder how to setup RTI for periodic interrupt. For example RTI8 for CR5_MAIN0_0.
I got the RTI setup correctly (borrowed from Hercules) but there seems to be no interrupt arriving at the VIM/VIC.
According to the manual, there is only one RTI interrupt at 0.
Do I have to enable the interrupt at some other place besides RTI and VIC?
Too bad, there are no RTI examples in the SDK.
Any tip?