This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can not install c6flo 2 plug-in into Linux CCS5.



I'm having problems installing C6flo 2 plug-in into the Linux version of CCS5.   I get the following errors..

----

Cannot complete the install because of a conflicting dependency.
  Software being installed: C6Flo Feature 3.1.0.201103241321 (com.ti.gde.adapter.c6flo.feature.group 3.1.0.201103241321)
  Software currently installed: Shared profile 1.0.0.1302875735653 (SharedProfile_epp.package.cpp 1.0.0.1302875735653)
  Only one of the following can be installed at once:
    DVT Core 3.1.0.201103241321 (com.ti.dvt.core 3.1.0.201103241321)
    DVT Core 3.0.0.201101131203 (com.ti.dvt.core 3.0.0.201101131203)
  Cannot satisfy dependency:
    From: Shared profile 1.0.0.1302875735653 (SharedProfile_epp.package.cpp 1.0.0.1302875735653)
    To: com.ti.dvt.core [3.0.0.201101131203]
  Cannot satisfy dependency:
    From: DVT Common Components 3.1.0.201103241321 (com.ti.dvt.common.feature.group 3.1.0.201103241321)
    To: com.ti.dvt.core [3.1.0.201103241321]
  Cannot satisfy dependency:
    From: C6Flo Feature 3.1.0.201103241321 (com.ti.gde.adapter.c6flo.feature.group 3.1.0.201103241321)
    To: com.ti.dvt.common.feature.group 3.1.0.201103241321

-----------------------------------------

 

Unfortunately I don't know wht any of those messages mean so I don't know how to proceed.

 

I'm using Ubuntu 10.4lst with all the latest update include an installation of mono.

The version of CCS5 is the current latest.  5.0.2.00006 found http://processors.wiki.ti.com/index.php/Category:Code_Composer_Studio_v5

Following instructions as specified in: http://processors.wiki.ti.com/index.php/C6Flo_2

Should this work?  If so what do I need to do?

Thanks,

 - Orlando

  • Orlando,

    Thank you for your interest in C6Flo 2.0 and for taking the time to report this problem.  We are aware of issues with installing and using the beta tool on Linux PCs, and we're working on an update that should solve these problems.  I expect that this update will be released within a week.  I will post an update to this thread when that happens.  Sorry for the inconvenience.