Other Parts Discussed in Thread: MSP430F2274, TMS320C6713B
Hi,
I'm new to the c6713 DSK. Currently, I'm using c6713 DSK to process some audio, and I need to use some external data from a peripheral chip (MSP430f2274) to enhance the audio processing. I have made the physical connection (using J1 - pin68, pin70, and pin72), and I have the slave code written in MSP430f2274. Now, I need to write a Master TX/RX code for c6713 DSK to pull data from MSP430f2274. However, I'm really stuck in writing the code for it, since I couldn't find any working examples for it. Does anyone have such a working example that you would like to share? Also, any comments or suggestions are welcome! I just need some help badly on this issue.
Thanks in advance!