How to run TSIP example on C6678 EVM?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TSIP on C667X devices
Requirements
Procedure

C:\ti\pdk_c667x_2_0_16\packages>pdksetupenv.bat
***************************************************
Environment Configuration:
***************************************************
SDK_INSTALL_PATH : C:/ti
PDK_INSTALL_PATH : C:/ti/pdk_c667x_2_0_16/packages
GMAKE_INSTALL_PATH : C:/ti/xdctools_3_55_02_22_core
PDK_SOC : c667x
PDK_VERSION : 2_0_16
RULES_MAKE : C:/ti/pdk_c667x_2_0_16/packages/ti/build/Rules.make
***************************************************
C:\ti\pdk_c667x_2_0_16\packages>pdkProjectCreate.bat C6678 all little tsip all dsp "C:\ti\pdk_c667x_2_0_16\packages"
=========================================================================
Configuration:
SOC : C6678
BOARD : all
ENDIAN : little
MODULE : tsip
PROJECT_TYPE : all
PROCESSOR : dsp
PDK_SHORT_NAME : "C:\ti\pdk_c667x_2_0_16\packages"
=========================================================================
Checking Configuration...
Complete
=========================================================================
PDK_PARTNO : C6678L
PDK_ECLIPSE_ID : com.ti.pdk.c667x
RTSC_PLATFORM_NAME : ti.platforms.evm6678
RTSC_TARGET : ti.targets.elf.C66
CCS_DEVICE : "com.ti.ccstudio.deviceModel.C6000.GenericC64xPlusDevice"
*****************************************************************************
Detecting all projects in PDK and importing them in the workspace "C:\ti\pdk_c667x_2_0_16\packages"\MyExampleProjects
Detected Test Project: TSIP_evmc6678_c66exampleProject
--------------------------------------------------------------------------------
Creating project 'TSIP_evmc6678_c66exampleProject'...
Done!

[C66xx_0] ************************************************** ********** TSIP Test Start *********************** ************************************************** Initialize application buffers. TSIP driver instance successfully initialized ----------------------- TSIP port 0 is powered up TSIP port instance successfully initialized TSIP port 0 super frame interrupt is registered Enabling TSIP timeslot TX 0x0 RX 0x0... TSIP timeslot TX 0x0 RX 0x0 successfully enabled Enabling TSIP timeslot TX 0x1 RX 0x1... TSIP timeslot TX 0x1 RX 0x1 successfully enabled Enabling TSIP timeslot TX 0x2 RX 0x2... TSIP timeslot TX 0x2 RX 0x2 successfully enabled Enabling TSIP timeslot TX 0x3 RX 0x3... TSIP timeslot TX 0x3 RX 0x3 successfully enabled Enabling TSIP timeslot TX 0x4 RX 0x4... TSIP timeslot TX 0x4 RX 0x4 successfully enabled Enabling TSIP timeslot TX 0x5 RX 0x5... TSIP timeslot TX 0x5 RX 0x5 successfully enabled Enabling TSIP timeslot TX 0x6 RX 0x6... TSIP timeslot TX 0x6 RX 0x6 successfully enabled Enabling TSIP timeslot TX 0x7 RX 0x7... TSIP timeslot TX 0x7 RX 0x7 successfully enabled Enabling TSIP timeslot TX 0x8 RX 0x8... TSIP timeslot TX 0x8 RX 0x8 successfully enabled Enabling TSIP timeslot TX 0x9 RX 0x9... TSIP timeslot TX 0x9 RX 0x9 successfully enabled Enabling TSIP timeslot TX 0xa RX 0xa... TSIP timeslot TX 0xa RX 0xa successfully enabled Enabling TSIP timeslot TX 0xb RX 0xb... TSIP timeslot TX 0xb RX 0xb successfully enabled Enabling TSIP timeslot TX 0xc RX 0xc... TSIP timeslot TX 0xc RX 0xc successfully enabled Enabling TSIP timeslot TX 0xd RX 0xd... TSIP timeslot TX 0xd RX 0xd successfully enabled Enabling TSIP timeslot TX 0xe RX 0xe... TSIP timeslot TX 0xe RX 0xe successfully enabled Enabling TSIP timeslot TX 0xf RX 0xf... TSIP timeslot TX 0xf RX 0xf successfully enabled Enabling TSIP timeslot TX 0x10 RX 0x10... TSIP timeslot TX 0x10 RX 0x10 successfully enabled Enabling TSIP timeslot TX 0x11 RX 0x11... TSIP timeslot TX 0x11 RX 0x11 successfully enabled Enabling TSIP timeslot TX 0x12 RX 0x12... TSIP timeslot TX 0x12 RX 0x12 successfully enabled Enabling TSIP timeslot TX 0x13 RX 0x13... TSIP timeslot TX 0x13 RX 0x13 successfully enabled Enabling TSIP timeslot TX 0x14 RX 0x14... TSIP timeslot TX 0x14 RX 0x14 successfully enabled Enabling TSIP timeslot TX 0x15 RX 0x15... TSIP timeslot TX 0x15 RX 0x15 successfully enabled Enabling TSIP timeslot TX 0x16 RX 0x16... TSIP timeslot TX 0x16 RX 0x16 successfully enabled Enabling TSIP timeslot TX 0x17 RX 0x17... TSIP timeslot TX 0x17 RX 0x17 successfully enabled Enabling TSIP timeslot TX 0x18 RX 0x18... TSIP timeslot TX 0x18 RX 0x18 successfully enabled Enabling TSIP timeslot TX 0x19 RX 0x19... TSIP timeslot TX 0x19 RX 0x19 successfully enabled Enabling TSIP timeslot TX 0x1a RX 0x1a... TSIP timeslot TX 0x1a RX 0x1a successfully enabled Enabling TSIP timeslot TX 0x1b RX 0x1b... TSIP timeslot TX 0x1b RX 0x1b successfully enabled Enabling TSIP timeslot TX 0x1c RX 0x1c... TSIP timeslot TX 0x1c RX 0x1c successfully enabled Enabling TSIP timeslot TX 0x1d RX 0x1d... TSIP timeslot TX 0x1d RX 0x1d successfully enabled Enabling TSIP timeslot TX 0x1e RX 0x1e... TSIP timeslot TX 0x1e RX 0x1e successfully enabled Enabling TSIP timeslot TX 0x1f RX 0x1f... TSIP timeslot TX 0x1f RX 0x1f successfully enabled TSIP Port 0 configured ----------------------- TSIP data transfer...
Thanks,
Rajarajan U