This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Android doesnt boot on BeagleBoard-XM

Hello there, I've trying to boot Android on my bb-xm, but it seems it can't boot at all Eclair nor Froyo.

I could manage to boot WINCE and ANGSTROM, my bb doesnt like android :(

 

Here is the LOG, could you guys help me?

 

The oldest data was removed. Continue...
core: registered new interface driver smsc95xx
usbcore: registered new interface driver gl620a
usbcore: registered new interface driver net1080
usbcore: registered new interface driver plusb
usbcore: registered new interface driver rndis_host
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver MOSCHIP usb-ethernet driver
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 3 ports detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
android init
android_probe pdata: c04d153c
android_bind
android_usb gadget: android_usb ready
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 2
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
f_adb init
android_register_function adb
adb_bind_config
f_mass_storage init
android_register_function usb_mass_storage
mice: PS/2 mouse device common for all mice
input: gpio-keys as /devices/platform/gpio-keys/input/input0
i2c /dev entries driver
Linux video capture interface: v2.00
mt9v113 2-003c: Registered to v4l2 master omap34xxcam!!
omap-iommu omap-iommu.0: isp: version 1.1
OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
mmci-omap-hs mmci-omap-hs.1: err -16 configuring card detect
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
logger: created 64K log 'log_main'
logger: created 256K log 'log_events'
logger: created 64K log 'log_radio'
logger: created 64K log 'log_system'
Advanced Linux Sound Architecture Driver Version 1.0.21.
usbcore: registered new interface driver snd-usb-audio
usb 1-2: new high speed USB device using ehci-omap and address 2
No device for DAI omap-mcbsp-dai-0
No device for DAI omap-mcbsp-dai-1
No device for DAI omap-mcbsp-dai-2
No device for DAI omap-mcbsp-dai-3
No device for DAI omap-mcbsp-dai-4
OMAP3 Beagle SoC init
asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok
ALSA device list:
  #0: omap3beagle (twl4030)
TCP cubic registered
NET: Registered protocol family 17
NET: Registered protocol family 15
Power Management for TI OMAP3.
Unable to set L3 frequency (400000000)
Switched to new clocking rate (Crystal/Core/MPU): 26.0/664/800 MHz
IVA2 clocking rate: 660 MHz
SmartReflex driver initialized
omap3beaglelmb: Driver registration complete
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omapdss DPI: Could not find exact pixel clock. Requested 23500 kHz, got 24000 kHz
regulator_init_complete: incomplete constraints, leaving VAUX3 on
regulator_init_complete: incomplete constraints, leaving VDVI on
regulator_init_complete: incomplete constraints, leaving VDAC on
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
mt9v113 2-003c: chip id mismatch read 0x0, expecting 0x2280
mt9v113 2-003c: Unable to detect decoder
mt9v113 2-003c: chip id mismatch read 0x0, expecting 0x2280
mt9v113 2-003c: Unable to detect decoder
mt9v113 2-003c: chip id mismatch read 0x0, expecting 0x2280
mt9v113 2-003c: Unable to detect decoder
mt9v113 2-003c: chip id mismatch read 0x0, expecting 0x2280
mt9v113 2-003c: Unable to detect decoder
omapdss DPI error: display already enabled
omap_vout omap_vout: 'dvi' Display already enabled
omapdss DPI error: display already enabled
omap_vout omap_vout: 'dvi' Display already enabled
omap_vout omap_vout: Buffer Size = 3686400
omap_vout omap_vout: : registered and initialized video device 0
omap_vout omap_vout: Buffer Size = 3686400
hub 1-2:1.0: USB hub found
omap_vout omap_vout: : registered and initialized video device 1
hub 1-2:1.0: 5 ports detected
Waiting 1sec before mounting root device...
mmc0: host does not support reading read-only switch. assuming write-enable.
mmc0: new high speed SDHC card at address 1234
mmcblk0: mmc0:1234 SA04G 3.67 GiB
 mmcblk0: p1 p2 p3
usb 1-2.1: new high speed USB device using ehci-omap and address 3
smsc95xx v1.0.4
usb0: register 'smsc95xx' at usb-ehci-omap.0-2.1, smsc95xx USB 2.0 Ethernet, 4a:48:d4:6a:9d:9e
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
Freeing init memory: 172K
Warning: unable to open an initial console.
init: cannot open '/initlogo.rle'
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
# enabling adb
adb_open
warning: `zygote' uses 32-bit capabilities (legacy support in use)

 

After this point the screen shows ANDROID boot logo and it just keeps refreshing, totally stuck, no action.

Could you guys help me? Thank you