This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359: Sample code for an FTP client

Part Number: AM3359

Hi experts,

Q1:Is there any sample code for an FTP client for AM335x (or Sitara)?

I see that the sample code for the FTP server is in the SDK. Any information would be appreciated.

[add]

Sorry for the additional questions.

Q2:In the case that there is no client sample, is it possible to make a connection request from the server side when the IP address, port number, and MAC address of the connection destination are known in the current FTP server sample?

If this is possible, I would appreciate it if you could share the sample code to request a connection from the server.

Best regards,
O.H