Hi TI,
I compile the csirx_capture_test example, and put binay csirx_capture_testapp_freertos_mcu2_0_release.xer5f to /lib/firmware, then link j7-main-r5f0_0-fw to it , reboot the system, but It seems it doesn't work, no related log output. thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
I compile the csirx_capture_test example, and put binay csirx_capture_testapp_freertos_mcu2_0_release.xer5f to /lib/firmware, then link j7-main-r5f0_0-fw to it , reboot the system, but It seems it doesn't work, no related log output. thanks.
Hi Veitch Kyrie,
We cannot run the CSI example from Linux. You need to keep the board in the no-boot mode and use CCS to load and run the example, as explained in section 6.3.2 in below link.
After connecting to Main_Cortex_R5, you could load CSI RX example and run it from there.
Regards,
Brijesh