Hello,
8.2 PLL Controllers from AM1808 Reference Guide(sprugm9a) says that "the system operates in bypass mode by default and the system clock (OSCIN) is provided directly from an input reference clock (square wave or internal oscillator) selected by the CLKMODE bit in PLLCTL".
However CLKMODE is default to internal oscillator.
If we run an external clock, is it Ok leaving CLKMODE=0?
Regards,
N.Shinozaki