Other Parts Discussed in Thread: AM5718
Hi experts,
My customer is designing a prototype board using the AM5706.
Q1:Is it possible for the AM5706 to use the SSC (Spread Spectrum Clocking) function for high-speed signal systems such as DDR and USB3.0?
In the following thread, AM5718 is able to do it, so I think it is possible, but please let me check just in case.
e2e.ti.com/.../2820329
Q2:Am I correct in saying that SSC can be used, but you will not get support from TI?
The following thread looked like SSC itself is not supported, not just SSC as DSS.
e2e.ti.com/.../am5708-video-dpll-ssc-support
Q3:The AM5706 TRM (spruhz7j.pdf) says "only available under proper licensing agreement", but if I want to use SSC, do I need a licensing agreement?
Sorry, but I don't have any knowledge about SSC, so I would appreciate it if you could tell me.
Best regards,
O.H